BeeKit Test Tool Fails to recognize the virtual comport (device)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BeeKit Test Tool Fails to recognize the virtual comport (device)

1,478 Views
greatbigman
Contributor I

Hello~~

 

I  installed Beekit 1.9.17 onto a  Windows 7.

When I launch Test tool from Beekit. The communication settings found no comport of my device (see attached picture). However, my device is shown in the Device manager window. My device is a SBR board  with CP2102 as the virtual comport interface.

 

I can use the same board to communicate with Hyperterminal or other serial program.

 

I wonder whether this is because of the CP2102's driver version. I am using the Silab driver included with Beekit. 

But Test tool failed to found my device as described above.

 

When I use the same board on another PC (with older version of CP2102). Everything work fine.

 

Please help....

Many thanks.

Labels (1)
0 Kudos
Reply
1 Reply

1,174 Views
Xarxas
Contributor I

I have the same problem. 

Try to run the Test Tool as Administrator and It will works with others virtual COM. :smileywink:

0 Kudos
Reply