Basic IIC information for HCS08 - Quick Reference User Guide?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Basic IIC information for HCS08 - Quick Reference User Guide?

1,796 Views
danielhembree
Contributor III

Is the information in the HCS08 Quick Reference User Guide a good place to start for developing IIC code, or is there a better resource? I have not used this module in the HCS08 and have no experience with IIC...yet.

 

Thanks,

Dan

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,524 Views
david_diaz
NXP Employee
NXP Employee

I recommend you the Application Note AN3291.

This application note is an example of how to use the IIC module on Freescale’s HCS08 MCUs. The IIC module can be used in the master or slave mode, respectively. In this case, the master mode communicates with the serial EEPROM because the IIC bus is used mainly for communication between an MCU and a IIC peripheral device.

Please find the document mentioned above in the following link:

http://www.freescale.com/files/microcontrollers/doc/app_note/AN3291.pdf

Hope this information will be useful for you.

Have a great day.

0 Kudos
Reply