BDM runs to slow when you slow down internal clock (QE4 + Multilink)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BDM runs to slow when you slow down internal clock (QE4 + Multilink)

1,145 Views
CarlFST60L
Senior Contributor II

Why when I slow down the internal clock on the QE4 does the BDM step time take FOREVER, its impossilby slow.

 

i.e. clock setting

  ICSC1 = 0b01000110;  //Slow internal clock For normal operation
  ICSC2 = 0;

Labels (1)
0 Kudos
Reply
1 Reply

629 Views
pgo
Senior Contributor V

Dear CalrIFST60L,

 

The internal clock is at around 35 kHz.  You would expect the BDM interface to be really sloooow if you change the bus clock to such a low value.  By default the BDM interface runs at the Bus clock (/2?).

 

Two possibilities

 

- You didn't actually mean to bypass the FLL  by changing the CLKS bits in the ICSC1.  If not, check your values (see 11.3.1 of the manual).

 

- Configure your BDM so that it sets the CLKSW bit in the BDCSCR register so that the BDM uses the alternative BDM clock (ICSLCLK ~ 8MHz).

 

bye

 

Message Edited by pgo on 2009-12-04 04:03 PM
0 Kudos
Reply