Assembly langauge code or C code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Assembly langauge code or C code

12,875 Views
venki
Contributor I
Hi,
I have source code read  from MC08GP32. can we convert these codes in assembly Langauge or C Language.
 
Venki
 
Message Edited by t.dowe on 2009-09-04 02:14 PM
Labels (1)
0 Kudos
Reply
25 Replies

1,323 Views
venki
Contributor I
Dear Peg,
Thanks for your valueble effort in confirming aboat the code.You have not mentioned anything aboat Code above assembly code.
 
Regards
venki
0 Kudos
Reply

1,323 Views
bigmac
Specialist III
Hello Venki,
 
Within the listing file, the first half of the file contains a "memory dump" of each line of the .S19 file, one line at a time.  It can be ignored, since your interest is with the disassembled code.
 
I am curious as to what you hope to achieve with the disassembly.
 
Once you have separated the code into the various sub-routines, identify those "low level" routines that do not call any other sub-routines.  Then attempt to identify what each of these does.  The routines that read or write peripheral registers may be easier to decode.  I suggest you add copious comments as you work through the code.
 
I also don't envy your task of making sense of about 27K of code - I have previously reverse engineered projects with about 1K to 2K of code that was originally written in assembler (and not compiled from C), and this was tedious and time consuming enough.
 
Regards,
Mac
 
0 Kudos
Reply

1,323 Views
Curt
Contributor IV
One thing for sure though Venki:  if you actually manage to dis-compile a 27K program you will be a bonafide expert in several areas (assembly language the least of them).
 
It will be a bit like trying to reconstruct your program from a listing that's been through the shredder twice -- or rewriting Kafka's  _The Trial_ given a box of the letters contained in the original book:smileyhappy:
0 Kudos
Reply

1,323 Views
Alban
Senior Contributor II
lst files are now allowed.
0 Kudos
Reply

1,323 Views
Curt
Contributor IV
Hi venki.
If you follow Peg's advice and can download a free "special edition" of CodeWarrior from the Freescale web site, you will not only get an assembler manual and tools -- but also a simulator that will let you practice writing, assembling and executing programs in assembly language.  
 
This is one of those "bargains" that will make you say -- "Wow!"
 
Regards,
Curt
0 Kudos
Reply