Anybody have data sheet for MC9S08DZ128

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Anybody have data sheet for MC9S08DZ128

4,588件の閲覧回数
anunalge
Contributor I
ラベル(1)
0 件の賞賛
返信
7 返答(返信)

2,801件の閲覧回数
Lundin
Senior Contributor IV
Is there even a 128k version of the DZ? When I spoke with Freescale just the other week, they said that 60k was the largest one.
0 件の賞賛
返信

2,801件の閲覧回数
JimDon
Senior Contributor III
Well according to that page, no there is not.
I figured he was mistaken about the 128 and the referenced page would answer that.

0 件の賞賛
返信

2,801件の閲覧回数
allawtterb
Contributor IV
At one point freescale had indicated that there would be a DZ128 at some point in the future but I am not sure if this is still the case.  I remember seeing it on a roadmap but it was an old document.
 
 
Document is from 2006 and shows the DZ with 96K and 128K options, I think these might have fallen out of favor with Freescale as all new documentation doesn't mention them.


Message Edited by allawtterb on 2008-02-29 03:24 PM
0 件の賞賛
返信

2,801件の閲覧回数
allawtterb
Contributor IV
Another note, in July of last year Freescale provided an update to CodeWarrior 6.0 to support the DZ96 and DZ128.  Perhaps these are still planned, but someone from Freescale would have to clear this up.
0 件の賞賛
返信

2,801件の閲覧回数
anunalge
Contributor I
I got the evaluation board from softec microsystems which consists of this controller.But datasheet is not available.
0 件の賞賛
返信

2,801件の閲覧回数
JimDon
Senior Contributor III
Datasheet for what?
The mcu, or the board?
Look here for the board.

The user guides and schematics are here.

See previous posted  link for the chip.


Message Edited by JimDon on 2008-03-28 10:28 AM
0 件の賞賛
返信

2,801件の閲覧回数
JimDon
Senior Contributor III
Look Here.

To find a part you would go to products/8-bit/ then pick the one you want off the left menu.

0 件の賞賛
返信