Allication Note & Code for to drive a LCD

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Allication Note & Code for to drive a LCD

2,004件の閲覧回数
eud
Contributor I

Hello

I'm working on a MC9RS08LA8 and I hvae to drive a LCD without LCD Controller. But the MC9RS08LA8 has an internal LCD Controler, but I didn't found an Appl. Note and C-Routine for this. The LCD is 1 line with 4 characters. Do you know any App. Note? I saw AN3796 but I think there are other ones?

Thanks

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,409件の閲覧回数
bigmac
Specialist III

Hello,

 

Did you also download the software associated with AN3796?  This software would appear to provide a good starting point for the low level LCD driver code that you require.  I guess that this will need to be adapted for the specific display that you are using.

 

I think that you will find that the majority of prior threads concern LCD modules with built-in driver hardware, rather than the operation of the internal hardware within the MCU device.

 

Regards,

Mac

 

0 件の賞賛
返信

1,409件の閲覧回数
J2MEJediMaster
Specialist I

Use the forum search function (text entry box at lower left of this page) and enter "LCD control". This topic has been discussed many times before.

 

---Tom

Message Edited by J2MEJediMaster on 2010-01-21 08:50 AM
0 件の賞賛
返信