Active Interruption of timer channel 0  in Code Warrior

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Active Interruption of timer channel 0  in Code Warrior

1,467 次查看
Johanny
Contributor I
I need active an interruption in Code Warrior for the Timer in the channel 0 when it finish the counting...i need to reset the program execution...
thanks...
标签 (1)
0 项奖励
回复
1 回复

774 次查看
Alban
Senior Contributor II
Hi,

As in all messages, you need to tell which device you are targetting.
And, for CodeWarrior questions, they should naturally be asked in the proper CodeWarrior board and specify which CodeWarrior version is used.

There is no universal answer to your question.

Regards,
Alban.
0 项奖励
回复