Active Interruption of timer channel 0  in Code Warrior

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Active Interruption of timer channel 0  in Code Warrior

1,834 Views
Johanny
Contributor I
I need active an interruption in Code Warrior for the Timer in the channel 0 when it finish the counting...i need to reset the program execution...
thanks...
Labels (1)
0 Kudos
Reply
1 Reply

1,141 Views
Alban
Senior Contributor II
Hi,

As in all messages, you need to tell which device you are targetting.
And, for CodeWarrior questions, they should naturally be asked in the proper CodeWarrior board and specify which CodeWarrior version is used.

There is no universal answer to your question.

Regards,
Alban.
0 Kudos
Reply