AN3927 problem device cannot start with JM60

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AN3927 problem device cannot start with JM60

1,944件の閲覧回数
eduardo1
Contributor II

Hello, i'm trying to use USB MSD bootloader with JM60 but when i connect the microcontroller to the HOST there is a message "device cannot start(code 10)" . Anyone had the same problem? How can i solve it?


I'm using Code warrior 6.3, AN3927 code reference and windows 10.

ラベル(1)
0 件の賞賛
返信
1 返信

1,871件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi 

The AN3927 is old, and there is not a new version for it, you can check the recommendation on the following thread

https://community.nxp.com/thread/318424 

Also codewarrior 6.3 is not recommended to run on windows 10, maybe you also have some problem with the windows driver

Regards

0 件の賞賛
返信