AN3927 problem device cannot start with JM60

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AN3927 problem device cannot start with JM60

1,965 Views
eduardo1
Contributor II

Hello, i'm trying to use USB MSD bootloader with JM60 but when i connect the microcontroller to the HOST there is a message "device cannot start(code 10)" . Anyone had the same problem? How can i solve it?


I'm using Code warrior 6.3, AN3927 code reference and windows 10.

Labels (1)
0 Kudos
Reply
1 Reply

1,892 Views
vicentegomez
NXP TechSupport
NXP TechSupport

Hi 

The AN3927 is old, and there is not a new version for it, you can check the recommendation on the following thread

https://community.nxp.com/thread/318424 

Also codewarrior 6.3 is not recommended to run on windows 10, maybe you also have some problem with the windows driver

Regards

0 Kudos
Reply