When it fails, the data from USBlyzer looks like this:
Connection Status Device connected
Current Configuration 0
Speed Low (1.5 Mbit/s)
Device Address 0
Number Of Open Pipes 0
Device Descriptor
Offset Field Size Value Description
0 bLength 1 12h
1 bDescriptorType 1 01h Device
2 bcdUSB 2 0200h USB Spec 2.0
4 bDeviceClass 1 00h Class info in Ifc Descriptors
5 bDeviceSubClass 1 00h
6 bDeviceProtocol 1 00h
7 bMaxPacketSize0 1 10h Should be 8 bytes for low-speed devices
8 idVendor 2 15A2h Freescale Semiconductor, Inc.
10 idProduct 2 003Fh
12 bcdDevice 2 0100h 1.00
14 iManufacturer 1 01h
15 iProduct 1 02h
16 iSerialNumber 1 00h
17 bNumConfigurations 1 01h