AN3048SW Update

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AN3048SW Update

2,087件の閲覧回数
kmdelbarba
Contributor I
I'm trying to work with IIC and looking at AN3048 for help but I can't seem to get it to compile. It says it needs to be updated to version 5 from 3.1 but I can't find the 3.1 version to do the updating that the updating pdf says I need to have. If someone could put up the updated AN3048SW or guide me to doing it. I'm also curious why old files are even up there still. Why aren't they updated?

Thanks,

Kris DelBarba
ラベル(1)
0 件の賞賛
返信
1 返信

1,202件の閲覧回数
bigmac
Specialist III
Hello Kris,
 
The simplest approach is probably to create a new project for CW5, and import the file QG_IIC_Master.c or QG_IIC_Slave.c into the project.  Each file will be found in the Sources folder of its respective CW3.1 project.
 
Regards,
Mac
 
0 件の賞賛
返信