AN3048SW Update

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AN3048SW Update

2,055 Views
kmdelbarba
Contributor I
I'm trying to work with IIC and looking at AN3048 for help but I can't seem to get it to compile. It says it needs to be updated to version 5 from 3.1 but I can't find the 3.1 version to do the updating that the updating pdf says I need to have. If someone could put up the updated AN3048SW or guide me to doing it. I'm also curious why old files are even up there still. Why aren't they updated?

Thanks,

Kris DelBarba
Labels (1)
0 Kudos
Reply
1 Reply

1,170 Views
bigmac
Specialist III
Hello Kris,
 
The simplest approach is probably to create a new project for CW5, and import the file QG_IIC_Master.c or QG_IIC_Slave.c into the project.  Each file will be found in the Sources folder of its respective CW3.1 project.
 
Regards,
Mac
 
0 Kudos
Reply