AN2295sw bootloader problem for MC9S08LH36

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

AN2295sw bootloader problem for MC9S08LH36

ソリューションへジャンプ
3,693件の閲覧回数
danielhou
Contributor II

hello, everybody,  I met a puzzle problem when I used AN2295sw in MC9S08LH36 microcontroller. According the application manual, first I download the S19 file of S08LH project in src folder, then I use win_hc08sprg.exe to open my program's S19 file in PC, when I click the connect, it hints error, unknown protocol version.

ラベル(1)
タグ(2)
0 件の賞賛
返信
1 解決策
3,304件の閲覧回数
danielhou
Contributor II

Monica, I didn't try to Samuel's suggestion, but I get the another solution from Freescale engineer. this solution includes a PC software and a bootloader file, I need add this bootloader file into my work and modify initial program in order to enter bootloader status. Finally, this solution can work. the following picture is PC software interface.

QQ截图20130510092116.jpg

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
3,304件の閲覧回数
sachin_k
Contributor I

Hi Daniel,


I am getting the same error .Can you please share Freescale Bootloader V1.2.3.exe file with me.


0 件の賞賛
返信
3,305件の閲覧回数
danielhou
Contributor II

Monica, I didn't try to Samuel's suggestion, but I get the another solution from Freescale engineer. this solution includes a PC software and a bootloader file, I need add this bootloader file into my work and modify initial program in order to enter bootloader status. Finally, this solution can work. the following picture is PC software interface.

QQ截图20130510092116.jpg

0 件の賞賛
返信
3,304件の閲覧回数
Monica
Senior Contributor III

Daniel, that's amazing!

Thanks for sharing the workaround! :smileyhappy:

Best regards,

Monica.

0 件の賞賛
返信
3,304件の閲覧回数
Monica
Senior Contributor III

Daniel, did this suggestion work?

We would like to know! :smileywink:

Regards!

0 件の賞賛
返信
3,304件の閲覧回数
danielhou
Contributor II

the detailed error information is shown as following, and I also try to download the merging S19 file from my program and S08LH, but it failed, please help me, thank you!

error.JPG

0 件の賞賛
返信
3,304件の閲覧回数
rabbit
Contributor III

Hi Daniel,

I get similar problem for K60 MCU. You need download the AN2295 firmware to your target MCU, then it can talk to the bootloader.

Good luck.

Samuel

0 件の賞賛
返信