ADC PROBLEM - MC908SQG4

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ADC PROBLEM - MC908SQG4

1,625件の閲覧回数
Cram
Contributor III

Hi,

 

I'm using the MC908SQG4 (pdip 8 pins) for adquire two volatge levels using the ADC module. I don't need and interruption during the normal opreration so I decide to use a polling software solution, and here begins the problem. I'm just debbuging some test code  just to verify the adquisition method, and when I start the conversion as soon as i choose the input channel the COCO flag is set to 1, and finish the conversion process without result (ok result equals 0) here is the code

 

ADC configuration:

 

void initCAD(){

    //0001 1000
    ADCCFG_ADICLK=0;
    ADCCFG_MODE=2; //10 --> 10 bits
    ADCCFG_ADLSMP=1;
    ADCCFG_ADIV=0;
    ADCCFG_ADLPC=0;
   
      ADCSC2=0x00;
   
    //0001 1111
    ADCSC1_ADCH=0x1F;   
    ADCSC1_ADCO=0;
    ADCSC1_AIEN=0;
   
    //0000 0011 PTAD0+PTAD1
        
    APCTL1=0x03;
}

 

main loop:

 

 for(;:smileywink: {
 
    delay1ms();
    
    ADCSC1_ADCH=0x01;   --> here I select CH0 or CH1    and COCO flag is SET  
    while (!ADCSC1_COCO) ;
   
    ADCSC1_ADCH=0x1F; --> disable de ADC module   
    resL=ADCRL;
    resH=ADCRH; 
 
 
  } /* loop forever */

 

Anybody can help me? I miss something but I'm not abble to find it!

 

 

Thx for all,

 

 

Added p/n to subject.

Message Edited by NLFSJ on 2009-03-19 12:36 PM
ラベル(1)
0 件の賞賛
返信
1 返信

971件の閲覧回数
bigmac
Specialist III

Hello,

 

Try reading the ADC result prior to disabling the ADC module.  Actually, there is no reason to disable the ADC module since the module will automatically revert to low power mode once each conversion is complete.

 

Regards,

Mac

 

0 件の賞賛
返信