AC32 SCI2 fail

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

AC32 SCI2 fail

5,338 次查看
wesleybrianez
Contributor I

Our customer uses a MC9S08AC32 SCI2 module (63/64 pin) for proprietary debugging issue.

We have TZ16649.1 / TZ16689.1 / TZ15938.1 LOT's causing intermittent failure parts here at his washer-machine application.

The AC32 from this LOT's does not working and the same PN when it come from other LOT works normally.

Is anyone knows if this LOT's has a problem?

Best regards,

Wesley

标签 (1)
0 项奖励
回复
7 回复数

5,147 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

I do not have any report of failures on the AC32 device.

Do you have a picture of the label or the body's mark in order to do a deep search on the internal system?

Regards

Vicente Gomez

0 项奖励
回复

5,143 次查看
wesleybrianez
Contributor I

Hi Vicente,

Many tks in advance.

Here i`ve attached one of our box label.

Best Regards,

Wesley Brianez

Wesley Brianez

Grupoitech | Enginering

+55 11 3350-0200

0 项奖励
回复

5,143 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Thanks 

We do not have a report of failures on these date code.

Can you have access to the SCI register in order to check if the device is properly programmed?

0 项奖励
回复

5,143 次查看
wesleybrianez
Contributor I

Our customer does not have the 'source code' or 'project file', only the '.bin' file.

This is a problem also because i can't troubleshoot it and these LOTs is causing intermittent failure at customer's washer-machine.

Is there anything I can do in this case?

BR,

Wesley

0 项奖励
回复

5,143 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Do you know if the customer is using the internal clock or an external clock, I am thinking that this can be the problem.

without the source code, there is not much that you can do. You can check if you can do an attache to the board, but if the device is secured you won't be able to perform the attached.

Regards

Vicente 

0 项奖励
回复

5,143 次查看
wesleybrianez
Contributor I

Well,

The EXTAL pin (58) drive a transistor, so they using internal clock.

The device is also protected... i tested it

Anymore we can do for troubleshooting?

0 项奖励
回复

5,143 次查看
vicentegomez
NXP TechSupport
NXP TechSupport

Without have access to the register, I do not have more ideas.

Sorry

0 项奖励
回复