AC128 - more Flash questions...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

AC128 - more Flash questions...

1,177 Views
LDAA_STAB
Contributor I

Looking through the AC 128 docs for information on vector relocation when Flash block protection is invoked.  Not finding anything I assume (!!) that the AC series does not have that particular function. 

Anybody know anything different? 

And, nyone know of a more up-to-date cache of AC series documents?

Have been using:  MC9S08AC128RM, Rev 3, 09/2008.

 

Thanks!

BillB

Labels (1)
0 Kudos
Reply
1 Reply

733 Views
bigmac
Specialist III

Hello Bill B.

 

I could not find any reference to automatic vector redirection either.  But perhaps this may be intentional?  There could be potentially very serious problems if the redirection location fell within the paging window.

 

I notice that the Reference Manuals for both 'AC60 and 'AC16 refer to vector redirection capability, although the 'AC60 places a limit on the amount of protected flash.

 

Regards,

Mac

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

 

/

0 Kudos
Reply