A question about GPIO on MC13213

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

A question about GPIO on MC13213

2,807件の閲覧回数
VincentLau
Contributor I
Hi,
   I am a newer on freescale 8-bit MCU. I know that all unused modem GPIOx should programmed as outputs in the low state when the MCU goes to Hibernate or Doze modes according to the document MC1321x.pdf on page 65. My question is that how can I operate on it, I have not seen any register about GPIO from any documents. I also check MC13213.h created automatically by Coderwarrior, but I have found nothing on it either.
  Can anyone help me? Thank you very much!
 
Best Regards
 
Vincent
Sep24,2008
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

1,765件の閲覧回数
Andrey
Contributor III
Basically when it refers to GPIO1-7 it  refers to a modem part

page 12 says
"The transceiver GPIO pins default to inputs at reset. There are no programmable pullups on these pins. Unused GPIO pins should be tied to ground if left as inputs, or if left unconnected, they should be programmed as outputs set to the low state. During low power modes, input must remain driven by MCU."

Take a look at MC1321xRM.pdf page 5-15 

gpio7_oen and so on.


Message Edited by Andrey on 2008-09-26 02:38 PM
0 件の賞賛
返信

1,765件の閲覧回数
Andrey
Contributor III
When it is talking about the GPIOx it means ANY general purpose input/output register (i.e. PTC7, PTC6...PTD3, PTE4)
For example, to set them as outputs in the low state use:
Code:
//PIN DIRECTION (1 == OUTPUT, 0 = INPUT)  PTADD_PTADD0 = 1; // CTRL1 // SHUTTER ELECTO-MAGNET//LEVEL ON THE PIN (FOR OUTPUTS ONLY)  PTAD_PTAD0 = 0; // LOW STATE
 Do that for all of the GPIOs that you don't use.
0 件の賞賛
返信

1,765件の閲覧回数
VincentLau
Contributor I
Hi, Andrey
 
   Thank you for your warmhearted reply! However, I see there are special GPIO1-4 on pin 44-41, and GPIO5-7 on pin 24-26 of MC13213 pinout. I don't know what they are.
 
Best Regards
 
Vincent
Set25,2008
0 件の賞賛
返信