9SC08QG4 TPM input capture and general input.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

9SC08QG4 TPM input capture and general input.

ソリューションへジャンプ
2,787件の閲覧回数
viking01
Contributor I

Hi

 

I'm using CodeWarrior in C to develop my software.

 

I've configured PTA0 on the 8pin device as an input capture (TPMCH0) input.  Can I still test the logic level on this pin by testing PTAD_PTA0 without having to change it to a General I/O first?

 

Also, I'm using interrupts to capture an input event, and saving the timer value to a variable (when the CH0F flag is set).  What is the difference between reading the TPMC0VH/L registers and TPMC0TH/L registers they appear to me to have the same information in them.  Is it a case that TPMC0VH/L is used for CH0F, and TPMC0TH/L is best used for T0F?

 

Thanks

viking01

ラベル(1)
0 件の賞賛
返信
1 解決策
1,686件の閲覧回数
viking01
Contributor I

Thanks bigmac,

 

Your assumption was correct, I did mean TPMCNT.  Thanks for your info and assistance.

 

Cheers

viking01

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,686件の閲覧回数
bigmac
Specialist III

Hello Viking01, and welcome to the forum.

 

In general, when a peripheral module is enabled, it will over-ride GPIO functionality.  I suspect this will also be the case for the input capture pin.

 

I think that you mean the TPMCNT (16-bit) register, compared with the TPMC0V register.

 

An input capture event will write the current contents of TPMCNT into the TPMC0V register, at the instant of the event.  Interrupt latency may then cause the two values to slightly differ at the time the interrupt is processed.  The true timer value for the capture event will therefore be that within TPMC0V.

 

Regards,

Mac

 

0 件の賞賛
返信
1,687件の閲覧回数
viking01
Contributor I

Thanks bigmac,

 

Your assumption was correct, I did mean TPMCNT.  Thanks for your info and assistance.

 

Cheers

viking01

0 件の賞賛
返信