9S08AW60 - Execution from protected flash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

9S08AW60 - Execution from protected flash

Jump to solution
4,910 Views
Skippy
Contributor II

Data Sheet:  MC9S08AW60 Data Sheet, Rev 2 implies in the last paragraph of  "4.4.6 FLASH Block Protection"  that a bootloader programmed into a protected section of FLASH is able to erase and program un-protected sections of FLASH.  To me this means that my FLASH programming functions can be executing out of flash and do not need to be relocated to RAM.  Any comments or experience in this area?

 

Thanks!

Labels (1)
0 Kudos
Reply
1 Solution
3,331 Views
Skippy
Contributor II

Word from above is that the FLASH array in 9s08AW60 is a single element. So, can't read and write indivisibly. Load the write functions to RAM and move forward.

 

View solution in original post

0 Kudos
Reply
6 Replies
3,331 Views
peg
Senior Contributor IV

Hi,

 

Unclearly written passages in datasheets WILL NOT change the characteristics or limitations of the flash memory used in these devices.

 

The limitation of not being able to execute from and write to flash in the same array at the same time remains.

0 Kudos
Reply
3,331 Views
Skippy
Contributor II

Hi Peg,

I know that "wishing doesn't make it so" and I have been reading and attempting to interpet Motorola/Freescale data sheets since the xc6800. Sometimes with pretty good results. Although in this case I think I got the answer from a local Arrow FAE.  He says "he thinks that if the sector, block, page or section  (choose your definition of a 512 byte FLASH block) is not protected and if the operational code is in a protected sector that the erase/burn functions should be able to live in that protected FLASH section".  IOW, don't try to program the block that is running code.

 

 

0 Kudos
Reply
3,331 Views
peg
Senior Contributor IV

Arrow FAE's "thinking" don't make it so either.

 

0 Kudos
Reply
3,331 Views
Skippy
Contributor II

Yes, well, we will wait, of course, to see what the lad has to say after he reads up on the official documents.

 

0 Kudos
Reply
3,332 Views
Skippy
Contributor II

Word from above is that the FLASH array in 9s08AW60 is a single element. So, can't read and write indivisibly. Load the write functions to RAM and move forward.

 

0 Kudos
Reply
3,331 Views
daveraymond
Contributor I
I believe your data sheet will say something like:

This bootloader program can call a routine outside of Flash that can be used to sector erase the rest of the Flash memory and reprogram it.

The key words are outside of Flash. That is our experience.

Dave Raymond

0 Kudos
Reply