802.15.4 PHY/MAC protocol stack for CodeWarrior V5.0

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

802.15.4 PHY/MAC protocol stack for CodeWarrior V5.0

2,141 次查看
Vianney
Contributor I
Hello.

First of all, I don't know if "8-Bit Microcontrollers forum" is the right place to post this message, if not, I'm sorry.

So, I wonder if there is a version of the "802.15.4 PHY/MAC protocol stack" for CodeWarrior V5.0. Now I am working with CodeWarrior V5.0 but I have only the version of the "802.15.4 PHY/MAC protocol stack" for CodeWarrior V3.1.
I have to convert and port too the stack, I have tried to do that but the issue of this work is not so good. So if someone have a suggestion reguard to the different versions of this protocol stack, it will be great.

Vianney
标签 (1)
0 项奖励
回复
1 回复

1,179 次查看
NLFSJ
Contributor III
Hi,
 

In answer to your question, if you are using the older MAC version, with 5.0 and it asks you to covert, just press cancel. The code will work fine.

You can upgrade to the latest version of the MAC that supports 5.0 by downloading the BeeKit. This is a GUI configuration program that contains the SMAC and MAC software.

http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=BEEKIT_WIRELESS_CONNECTIVITY_TOOLKIT&...

Regards,

Nina

0 项奖励
回复