8-Bit Architecture

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

8-Bit Architecture

3,573件の閲覧回数
admin
Specialist II
Hello  All,
                My doubt is whether all 8-bit freescale microcontrollers are having Von Neumann architecture.
ラベル(1)
0 件の賞賛
返信
3 返答(返信)

2,103件の閲覧回数
admin
Specialist II
Hello Peg,
                  I am preparing for a seminar on Freescale architecture,and I came across different cores like
S08, RS08 ,HC08,HC11 etc .When I read  different documents ,I could find that all are VonNeumann .But for others like PIC ,ATMEL there are 8-bit controllers  with Harvard architecture.So to clarify the doubts only I posted this.
                               So the conclusion is like all are VonNeumann architecture.
0 件の賞賛
返信

2,103件の閲覧回数
peg
Senior Contributor IV
Hello thunderbolt,

Which devices in particular are causing this doubt?
Given that there is only two cores in current use (HC08 and S08) I fail to see where it may be coming from.



Message Edited by peg on 2009-02-03 08:36 AM
0 件の賞賛
返信

2,103件の閲覧回数
fabio
Contributor IV
Hello Thunder,

AFAIK all 8-bit MCUs from Freescale are CISC and Von Neumann devices.

Best,
0 件の賞賛
返信