8-Bit Architecture

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

8-Bit Architecture

3,578 Views
admin
Specialist II
Hello  All,
                My doubt is whether all 8-bit freescale microcontrollers are having Von Neumann architecture.
Labels (1)
0 Kudos
Reply
3 Replies

2,108 Views
admin
Specialist II
Hello Peg,
                  I am preparing for a seminar on Freescale architecture,and I came across different cores like
S08, RS08 ,HC08,HC11 etc .When I read  different documents ,I could find that all are VonNeumann .But for others like PIC ,ATMEL there are 8-bit controllers  with Harvard architecture.So to clarify the doubts only I posted this.
                               So the conclusion is like all are VonNeumann architecture.
0 Kudos
Reply

2,108 Views
peg
Senior Contributor IV
Hello thunderbolt,

Which devices in particular are causing this doubt?
Given that there is only two cores in current use (HC08 and S08) I fail to see where it may be coming from.



Message Edited by peg on 2009-02-03 08:36 AM
0 Kudos
Reply

2,108 Views
fabio
Contributor IV
Hello Thunder,

AFAIK all 8-bit MCUs from Freescale are CISC and Von Neumann devices.

Best,
0 Kudos
Reply