68HC805K3 Programming

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

68HC805K3 Programming

3,610件の閲覧回数
colinh
Contributor I
Heres a blast from the past - the 68HC805K3
 
Does anyone have access to the programming instructions for directly programming the above, ie pins, signals, voltages, commands etc.  The original Rev 1 datasheet did not include this information.  As a "Plan Z" I need to investigate making up a programmer to get a client out of a bind. 
 
In case you're wondering why we need to do this - Our client has a current mask part (68HC05K3) and they need to trial new peeprom settings.  The mask part has the peeprom pre-programmed and secured at Freescale so we cant demo the peeprom changes with the mask parts.  The 805K3 is no longer manufactured but we have access to a small stock into which we need to program code/peeprom . 
 
Thanks
Colin
 
ラベル(1)
0 件の賞賛
返信
4 返答(返信)

1,790件の閲覧回数
Alban
Senior Contributor II
Hi Colin,
 

705K1 General Programming Information

This device does not have built-in bootloader ROM code. To program this device it must be put into expanded test mode. The user can either sign an NDA to get the test mode spec or use the M68HC705KICS Board to program these devices.

Do you have such NDA or the ICS ?

Cheers,
Alban {old stuff specialist}

0 件の賞賛
返信

1,790件の閲覧回数
colinh
Contributor I
Hi Alban

My client is Bosch (Australia). I have a confidentiality agreement with them, and they in turn have an NDA with Freescale. I have tried to send you a personal email with the details of a Freescale person who can co-ordinate this stuff. Please let me know via the forum if this is OK or otherwise

Regards
Colin
0 件の賞賛
返信

1,790件の閲覧回数
Alban
Senior Contributor II
Thanks Colin,
 
I'm in contact and will follow the matter up offline.
HC05K3 is quite an old product and I have to admit that I struggle to find information...
I have a few things I forwared to people dealing with your official enquiry (= not in forums).
 
Regards,
Alban.
0 件の賞賛
返信

1,790件の閲覧回数
Alban
Senior Contributor II
A few files for archive and Google's thirst of knowledge.
 
ICS05KW - Windows Help file
 
805K3ICSUM - ICS05 for 805K family user guide.
 
Alban.
 
Message Edited by t.dowe on 2009-09-22 11:25 AM
0 件の賞賛
返信