1321x: One Balun or Two?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1321x: One Balun or Two?

1,777 Views
glowbrain
Contributor I
Has anyone doen a comparison between the one and two balun solutions shown in the freescale reference designs? It would be interesting to know the advantages and disadvantages.
I cant imagine going to the one balun solution for the sake of price alone (a few cents worth of components) if the performance were severly compromised.
On the other hand, if the performance is similar, why bother with the two balun solution?
Labels (1)
0 Kudos
Reply
1 Reply

1,211 Views
Alex_RUS
Contributor I
I tasted boards whith 2 baluns and boards with 1 balun. I did not meter dbms but I can say that boards with 2 baluns about 20% more effective.
0 Kudos
Reply