13192DSK-BDM-A00 - How to reload software ?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

13192DSK-BDM-A00 - How to reload software ?

1,277 次查看
DrStefanFrank
Contributor I

Hello,

I got the one of the 13192DSK-BDM-A00 board here in my office and I tried the demo without any success, so I think the firmware is broken - what is the easiest way to get the demo-firmware back into the board ? I can't find the software and I am confused what kind of additional software it will need to get the boards running again - can you give me a step-by-step documentation ?

thanx a lot
Daniel

(Alban: thread split + subject update)

Message Edited by Alban on 2007-03-06 02:36 PM

标签 (1)
0 项奖励
回复
1 回复

748 次查看
peg
Senior Contributor IV
Hi DrStefanFrank,
 
There is not too many options here anyway.
Here is a rough run down.
Load Codewarrior on to a PC
Plug the USB-BDM into the USB port and the 6 pin ribbon onto the 6 pin header on the PCB.
Turn on the PCB
Fire up Codewarrior
Load the Codewarrior project that you want to try out into CW
press the little green bug.
This will compile it, erase the FLASH and then programme the application into the FLASH in the microcontroller on the PCB. From here you can run it in the simulator or unplug the ribbon and run it standalone (if thats what the project is meant to do).
If you are a real newbie, there is probably about 87 steps that I have left out!
Good Luck!
 
0 项奖励
回复