115200 on MC9S08QE128 with a high bus and system clock

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

115200 on MC9S08QE128 with a high bus and system clock

1,144 Views
Limestone
Contributor III

Hi!

 

I am developing a system that will need to communicate at 115200 in the temperature span of +20 to +70 celcius. As internal oscillator are known to be temperature dependent, I guess I have to use an external crystal (Correct?). I also need a fairly fast bus clock and system clock.

 

Right now, during development, I am using the internal oscillator at 36 kHz, trimmed it during programming to 36 kHz. I have a bus clock of ~18 MHz and and a FLL output clock of ~36 MHz.

 

I can use the same values with an external crystal that matches the internal oscillator. A 36 kHz crystal, but as they are about ten times as expensive as for instance a 3,6864 cyrstal, I wonder if there are any other settings (using a more common crystal) that will allow me to have a relative high system speed and 11520 baud rate.

 

Best regards

Martin

Labels (1)
0 Kudos
Reply
1 Reply

637 Views
tonyp
Senior Contributor II

You can get usable 115K baud even with the internal oscillator, if you trim the device.  By the datasheet, the oscillator deviation percentage (2%) is valid throughout the operating temp range.  So, you should be OK.  Still, you may want to use a crystal for lower noise.

 

I like the 4MHz [or 8MHz] crystal which after dividing down (RDIV) by 128 [or 256] (for 31.25KHz base frequency) and using the 1536 FLL multiplier, you get 48MHz (24MHz bus) which is near the top end of the specs, and also provides exact real-time clock.

 

0 Kudos
Reply