I want to play some music or movic by Qt. So first I use QMediaPlayer to do that, it isn't working, with message:
defaultServiceProvider::requestService(): no service found for - "org.qt-project.qt.mediaplayer"
After that, I try using QSoundEffect to do. The result is still the same but with message:
PulseAudioService: pa_context_connect() failed
But when I used the test project from /usr/share/qt5/examples/multimedia/imxplayer, it works well!!!
root@imx6qsabresd:/usr/share/qt5/examples/multimedia/imxplayer# ./imxplayer
** Message: GStreamer version 1.8.1
display(/dev/fb0) resolution is (1024x768).
Then I try running pulseaudio Individually on root:
W: [pulseaudio] main.c: This program is not intended to be run as root (unless --system is specified).
E: [pulseaudio] module-console-kit.c: GetSessionsForUnixUser() call failed: org.freedesktop.DBus.Error.Spawn.PermissionsInvalid: The permission of the setuid helper is not correct
E: [pulseaudio] module.c: Failed to load module "module-console-kit" (argument: ""): initialization failed.
E: [pulseaudio] main.c: Module load failed.
E: [pulseaudio] main.c: Failed to initialize daemon.
If it's on other normal user, just without the warning.
Then I try pulseaudio -vvvv, there is so much message but with the same error message.
I spent a lot of time asking questions between Qt forum and here.So could somebody please tell me how to fix it in detail?