Hi Can you please confirm if iMX 6 solo can support 800MHz clock rate DDR3. Various test conditions are given on 400MZ and in block diagram it is shown as 400MHZ.
Hi Yuri
This is my first processor based design. Can you give me some link for selection of DDR3 which help me select new replacement part of existing DDR3.
Can you let me know if MT41K256M16TW-107:P will work with iMX solo.
Hello,
i.MX6S provides a 32/64-bit DDR3/DDR3L/LPDDR2-800 memory interface.
This means DDR clock frequency of 400 MHz.
Regards,
Yuri.