imx6q, gpio Current drive strength

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6q, gpio Current drive strength

2,117 Views
barakbarak
Contributor I

Hi,

if i use only one GPIO at 3.3V in the IMX6Q , can it drive to  3mA ?

I read the data sheet and it is not clear from their whether it is possible.

Regards, Barak

Labels (2)
0 Kudos
Reply
1 Reply

1,517 Views
Yuri
NXP Employee
NXP Employee

Hello,

  from the linked below Community thread :

 

  The GPIO buffer load capacity is not specified in units of current. It is specified in terms of buffer

drive strength or output impedance; refer to the Section "GPIO Output Buffer Impedance" of the i.MX6

Data Sheet(s).

 

what is value of GPIO source/sink current per pin on i.MX6? 

 

IBIS models may be used to estimate current.

 

https://community.nxp.com/message/395489 

 

I looked at i.MX6Q IBIS file - 3 mA may be provided by i.MX6, assuming proper

GPIO drive strength and external impedance are selected.

 

   Also, the total load current and power dissipation should be taken into account when calculating the

GPIO power budget.

 

Have a great day,
Yuri

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply