Problem using S32DS of debug and debug_ram

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem using S32DS of debug and debug_ram

3,603件の閲覧回数
jerrytomlee
Contributor II

__attribute__ ((section(".text")))
int main(void)
{
      int counter = 0;
      short int your = 0;

I have add a declaration of  "short int your = 0;"  in the example  "eTimer_MPC5744P" in S32DS.

I am using the newest S32DS 2017 R1 .

In debug model, it works well.

In debug_Ram model, it didn't work.

The Disassembly showed:

236 short int your = 0;
40002d00: se_li r7,0
40002d02: se_sth r7,12(r31)

And it failed at se_sth every time,and it show  No source available kind of things.

So I wonder why?

ラベル(2)
2 返答(返信)

3,225件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello Jerry,

the problem is hidden in startup code. When you run example from flash, local DMEM is initialized by startup code. In this part of memory is placed stack, which is used for local variable storing.

But when you run example from RAM, this part of memory is not initialized because there is conditional compilation. When you try to write half word (short int) into uninitialized memory, ECC error is created.

Please use the following part of startup, instead of original one:

 #ifdef START_FROM_FLASH

;#***************************** Initialise SRAM ECC ***************************/
;# Store number of 128Byte (32GPRs) segments in Counter
 e_lis       r5, __SRAM_SIZE@h  # Initialize r5 to size of SRAM (Bytes)
 e_or2i      r5, __SRAM_SIZE@l
 e_srwi      r5, r5, 0x7         # Divide SRAM size by 128
 mtctr       r5                  # Move to counter for use with "bdnz"

;# Base Address of the internal SRAM
 e_lis       r5, __SRAM_BASE_ADDR@h
 e_or2i      r5, __SRAM_BASE_ADDR@l

;# Fill SRAM with writes of 32GPRs
sram_loop:
    e_stmw      r0,0(r5)            # Write all 32 registers to SRAM
    e_addi      r5,r5,128           # Increment the RAM pointer to next 128bytes
    e_bdnz      sram_loop           # Loop for all of SRAM

#endif

;#************************ Initialise Local Data SRAM ECC *********************/
;# Store number of 128Byte (32GPRs) segments in Counter
 e_lis       r5, __LOCAL_DMEM_SIZE@h  # Initialize r5 to size of SRAM (Bytes)
 e_or2i      r5, __LOCAL_DMEM_SIZE@l
 e_srwi      r5, r5, 0x7         # Divide SRAM size by 128
 mtctr       r5                  # Move to counter for use with "bdnz"

;# Base Address of the Local SRAM
 e_lis       r5, __LOCAL_DMEM_BASE_ADDR@h
 e_or2i      r5, __LOCAL_DMEM_BASE_ADDR@l

;# Fill Local SRAM with writes of 32GPRs
ldmem_loop:
    e_stmw      r0,0(r5)            # Write all 32 registers to SRAM
    e_addi      r5,r5,128           # Increment the RAM pointer to next 128bytes
    e_bdnz      ldmem_loop          # Loop for all of SRAM

In original startup code, #endif is placed below ldmem_loop section.

Regards,

Martin

3,225件の閲覧回数
jerrytomlee
Contributor II

Thanks a lot for your help!

0 件の賞賛
返信