Can't access http://gnuarmeclipse.sourceforge.net/updates for KDS update

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't access http://gnuarmeclipse.sourceforge.net/updates for KDS update

5,276 Views
christophevigny
Contributor II

I'm trying to update my KDS version but it fails due to the unavailability of http://gnuarmeclipse.sourceforge.net/updates. Is there a workaround?

Thanks

0 Kudos
Reply
2 Replies

4,702 Views
BlackNight
NXP Employee
NXP Employee

Christophe,

the issue is because stronger encryption for the SourceForge web site (see GNU ARM Eclipse plug-ins: Received fatal alert: handshake_failure ). The best workaround (which worked for me) is to download the zip file (as pointed out by Alice) and install it from there.

Erich

0 Kudos
Reply

4,702 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello ,

The workaround is :

- Download the .zip file from GNU ARM Eclipse Plug-ins Releases 

- Then install it in KDS : help-> install new software -> Add->

pastedImage_2.png

select the .zip file to install .

Hope it helps


Have a great day,
Alice Yang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply