MFGTool for downloading IMX6DL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MFGTool for downloading IMX6DL

Jump to solution
3,388 Views
puchen
Contributor I

Hello

I  download the "Mfgtools-Rel-4.1.0_130816_MX6DL_UPDATER.tar.gz",but my board is eMMC5.0.

so there accours an error"mmc0: unrecognised EXT_CSD revision 7",so I had to built a new uImage.

But the uImage I built seems  have no utp device,I don't know why!

Here is my Log:

mxc_dvfs_core_probe

mmc0: new high speed DDR MMC card at address 0001

mmcblk0: mmc0:0001 861000 6.92 GiB

mmcblk0boot0: mmc0:0001 861000 partition 1 4.00 MiB

DVFS driver module loaded

mmcblk0boot1: mmc0:0001 861000 partition 2 4.00 MiB

mmcblk0: p1 p2 p3 p4 < p5 p6 p7 >

regulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on

regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on

regulator_init_complete: PFUZE100_VGEN2: incomplete constraints, leaving on

regulator_init_complete: PFUZE100_VGEN1: incomplete constraints, leaving on

mmcblk0boot1: unknown partition table

regulator_init_complete: SPKVDD: incomplete constraints, leaving on

snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)

Freeing init memory: 512K

mmcblk0boot0: unknown partition table

Starting UTP

ln: /etc/mtab: File exists

disable turn off display

Starting the hotplug events dispatcher udevd

udevd (2002): /proc/2002/oom_adj is deprecated, please use /proc/2002/oom_score_adj instead.

Synthesizing initial hotplug events

uuc 0.4 [built Aug 16 2013 01:24:08]

UTP: Waiting for device to appear

>>it stuck at here

Labels (1)
0 Kudos
Reply
1 Solution
3,016 Views
puchen
Contributor I

I had resolve this problem,UTP need configed at menuconfig

View solution in original post

0 Kudos
Reply
2 Replies
3,017 Views
puchen
Contributor I

I had resolve this problem,UTP need configed at menuconfig

0 Kudos
Reply
3,016 Views
igorpadykov
NXP Employee
NXP Employee

Hi pu

please recheck building options with attached Linux Guide

sect.3.9 Building Manufacturing Firmware, also

one can check if USB_ID signal is floating or high.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------