Hello
I download the "Mfgtools-Rel-4.1.0_130816_MX6DL_UPDATER.tar.gz",but my board is eMMC5.0.
so there accours an error"mmc0: unrecognised EXT_CSD revision 7",so I had to built a new uImage.
But the uImage I built seems have no utp device,I don't know why!
Here is my Log:
mxc_dvfs_core_probe
mmc0: new high speed DDR MMC card at address 0001
mmcblk0: mmc0:0001 861000 6.92 GiB
mmcblk0boot0: mmc0:0001 861000 partition 1 4.00 MiB
DVFS driver module loaded
mmcblk0boot1: mmc0:0001 861000 partition 2 4.00 MiB
mmcblk0: p1 p2 p3 p4 < p5 p6 p7 >
regulator_init_complete: PFUZE100_VGEN6: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN3: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN2: incomplete constraints, leaving on
regulator_init_complete: PFUZE100_VGEN1: incomplete constraints, leaving on
mmcblk0boot1: unknown partition table
regulator_init_complete: SPKVDD: incomplete constraints, leaving on
snvs_rtc snvs_rtc.0: setting system clock to 1970-01-01 00:00:00 UTC (0)
Freeing init memory: 512K
mmcblk0boot0: unknown partition table
Starting UTP
ln: /etc/mtab: File exists
disable turn off display
Starting the hotplug events dispatcher udevd
udevd (2002): /proc/2002/oom_adj is deprecated, please use /proc/2002/oom_score_adj instead.
Synthesizing initial hotplug events
uuc 0.4 [built Aug 16 2013 01:24:08]
UTP: Waiting for device to appear
>>it stuck at here
解決済! 解決策の投稿を見る。
I had resolve this problem,UTP need configed at menuconfig
Hi pu
please recheck building options with attached Linux Guide
sect.3.9 Building Manufacturing Firmware, also
one can check if USB_ID signal is floating or high.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------