To use i.MX6DQ SDIO with 1.8V/25MHz (not UHS).

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

To use i.MX6DQ SDIO with 1.8V/25MHz (not UHS).

ソリューションへジャンプ
3,110件の閲覧回数
satoshishimoda
Senior Contributor I

Hi community,

Our customer have a question about i.MX6DQ SDIO.

They want to use SDIO with 1.8V to connect a Wi-Fi module.

Then, I found the following posts talk about 1.8V SD/MMC.

How to enable UHS mode for SD card in u-boot_201304

supporting SDR104 in imx6 board by yocto

But I feel the solutions in these posts are the one for when use the SABRE AI schematics.

Our customer don't need SD voltage switching and UHS, and will use 1.8V SDIO with 25MHz.

In this case, what is required to use SDIO = 1.8V?

Best Regards,

Satoshi Shimoda

ラベル(6)
タグ(2)
0 件の賞賛
返信
1 解決策
2,584件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

it is sufficient to power i.MX6 NVCC_SDx (providing power for this

interface) with 1.8V.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,585件の閲覧回数
igorpadykov
NXP Employee
NXP Employee

Hi Satoshi

it is sufficient to power i.MX6 NVCC_SDx (providing power for this

interface) with 1.8V.

Best regards

igor

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
2,584件の閲覧回数
satoshishimoda
Senior Contributor I

Hi Igor,

> it is sufficient to power i.MX6 NVCC_SDx (providing power for this

> interface) with 1.8V.

Good.

Thank you for your prompt support.

Best Regards,

Satoshi Shimoda

0 件の賞賛
返信