Kinetis K8 FlexIo max serial clock speed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Kinetis K8 FlexIo max serial clock speed

4,214件の閲覧回数
AlainRIMLINGER
Contributor I

Hello. I would like to connect K8x Kinetis secure licrocontroller with SPI at higher rate than 24MHz. Can I use FlexIo interface to achieve this ? What would be the max speed of the FlexIO interface serial clock ? Thank you very much. Regards

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

3,690件の閲覧回数
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Alain RIMLINGER,

     From the K8X datasheet, you may know, the SPI operation frequent is 30Mhz, I don't know what the SPI frequent you want to achieve.

    If you want to use the FlexIO,  the clock speed may be higher, because the  FlexIO clock can up to 150Mhz.

    More detials about the FlexIO, please refer to this post:

Understanding FlexIO

Wish it helps you!

If you still have question, please contact with me!

Have a great day,

Jingjing

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

3,689件の閲覧回数
AlainRIMLINGER
Contributor I

Hello

Thank you very much.

It will help win the socket for NXP.

With best regards, Alain

Alain Rimlinger

Field Application Engineer

Arrow Electronics

13-15 rue du Pont des Halles

94656 Rungis Cedex

T +33 1 49 78 49 25

M +33 6 86 53 35 52

[email protected]<mailto:[email protected]>

www.arrow.com<http://www.arrow.com/>;

De : kerryzhou

Envoyé : mardi 16 février 2016 06:10

À : Alain Rimlinger

Objet : Re: - Kinetis K8 FlexIo max serial clock speed

NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Kinetis K8 FlexIo max serial clock speed

reply from Jingjing Zhou<https://community.freescale.com/people/kerryzhou?et=watches.email.thread> in Kinetis Microcontrollers - View the full discussion<https://community.freescale.com/message/614738?et=watches.email.thread#614738>

0 件の賞賛
返信