Second imprecise external abort causes the cpu to hang.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Second imprecise external abort causes the cpu to hang.

2,501 次查看
colepeterson
Contributor I

Hello,

My company is working on creating a robust system that can handle our Xilinx Kintex 7 going offline without taking Linux with it. Unfortunately, If we take a working system and unconfigure the fpga while writing to the pcie space we get a series of events that cause the cpu to hang. Any help is greatly appreciated!

Fault sequence.

1)The Fpga is unconfigured

2)The mmaped pcie space is no longer valid and throws a  imprecise external abort on the next write.

3)The default abort handler is called in drivers/pci/host/pci-imx6.c (imx6q_pcie_abort_handler()).

4)The default abort handler returns 0 "abort Handled".

5)The next write to the fpga's pcie space causes the cpu to hang.

We are working on tracking this down with the Dstream debugger but so far no luck.

CPU: Arm IMX6Q

FPGA: Xilinx Kintex 7

Kernel: freescale 3.10.53

标签 (2)
0 项奖励
回复
3 回复数

1,830 次查看
wooosaiiii
Contributor IV

Hello Cole Peterson,

did you managed to solve this issue?

We have a similar problem with iMX6Q hanging itself while we take down EP without notice.

Any advice would be welcomed.

Regards,

Primož 

0 项奖励
回复

1,830 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Cole

one can check patch below for imprecise abort issue

Gmane Loom

[PATCH v6 3/3] PCI: imx6: Add support for i.MX6 PCIe controller

Best regards

igor

0 项奖励
回复

1,830 次查看
colepeterson
Contributor I

Hello Igor,

Thank-you for the response but unfortunately the patch doesn't help. The abort handler is not called on step 5 when the cpu hangs.

-Cole

0 项奖励
回复