MQX with Processor Expert using KDS on FRDM-K64F?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MQX with Processor Expert using KDS on FRDM-K64F?

2,231 Views
kcw
Contributor III

Is it possible to setup a MQX project with Processor Expert enabled using KDS and run it on frdm-k64f?

Tags (1)
0 Kudos
Reply
3 Replies

1,906 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

Check this one : https://community.freescale.com/thread/330292

Regards,

Luis

0 Kudos
Reply

1,906 Views
kcw
Contributor III

Are the LDD the same as in Code Warrior?

I am trying to reuse an application coded with Code Warrior. I need access to the same LDD(ie CAN_LDD.h)

0 Kudos
Reply

1,906 Views
LuisCasado
NXP Employee
NXP Employee

Hello,

That threat I think, it is using PE to configure KSDK drivers. Derek Snell , can you please confirm?

Unfortunately, the MQX 4.1.1 doesn't have bsp projects with PE enabled for the KDS.

But in the case of MQX for KSDK, you can use PE to configure the KSDK drivers and perhaps use the non KSDK components (LDD) at the same time. I have never tried that. You could try.

Regards,

0 Kudos
Reply