Vybird, RGB888 input, RGB888 output, no quality lost???

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Vybird, RGB888 input, RGB888 output, no quality lost???

Jump to solution
3,709 Views
alfred_liu
NXP Employee
NXP Employee


Hi, Vybrid expert:

the actual limitaion is ITU decoder, which can only output YUV422 or YUV444 (actually from YUV422). 

so even we can input RGB888 and output RGB888, the quality will lost. right?

do we have anyway to do this without quality lost?

here is the information in our datasheet:

57.5.3 Decoder

The ITU Decoder block (2) detects the ITU656 timing reference signal (consists of a

four-word sequence in the following format: FF-00-00-XY) and extracts HSYNC,

VSYNC, field number signals and video data from the ITU data stream. The format of

active pixel data from the ITU stream is YUV 4:2:2. The decoder block can directly send

out this YUV 4:2:2 data, or interpolate it to YUV 4:4:4 format and send it out. This is

determined by the MODE444 field in the SCR register. This bit shall be set if the downscaler

is enabled, because the down-scaler works on YUV 4:4:4 data format.

0 Kudos
Reply
1 Solution
2,805 Views
kef2
Senior Contributor V

Skiping IOMUXC configuration, you need to set up just few registers like below. I have no hardware to verify RGB888 settings, hope it works.

VIU3->SCR =   VIU3_SCR_MODE32BIT_MASK   * 1  // 32 bit mode
      | VIU3_SCR_ROUND_ON_MASK    * 0
      | VIU3_SCR_DITHER_ON_MASK   * 0
      | VIU3_SCR_DMA_ACT_MASK     * 0
      | VIU3_SCR_SCALER_EN_MASK   * 0
      | VIU3_SCR_YUV2RGB_EN_MASK  * 0
      | VIU3_SCR_BC_EN_MASK       * 0
      | VIU3_SCR_MODE444_MASK     * 0  // YUV444 vs YUV422
      | VIU3_SCR_ERROR_IRQ_MASK   * 0
      | VIU3_SCR_DMA_END_IRQ_MASK * 0
      | VIU3_SCR_VSTART_IRQ_MASK  * 0
      | VIU3_SCR_HSYNC_IRQ_MASK   * 0
      | VIU3_SCR_VSYNC_IRQ_MASK   * 0
      | VIU3_SCR_FIELD_IRQ_MASK   * 0
      | VIU3_SCR_ECC_EN_MASK      * 0
      | VIU3_SCR_ERROR_EN_MASK    * 0
      | VIU3_SCR_DMA_END_EN_MASK  * 0
      | VIU3_SCR_VSTART_EN_MASK   * 0
      | VIU3_SCR_HSYNC_EN_MASK    * 0
      | VIU3_SCR_VSYNC_EN_MASK    * 0
      | VIU3_SCR_FIELD_EN_MASK    * 0
      | VIU3_SCR_FORMAT_CTRL_MASK * 0 // replace 0 with required RGB888 byte order setting
      | VIU3_SCR_SOFT_RESET_MASK  * 0
                 ;

VIU3->DMA_ADDR = VIDEO_BASE; // address to store image data

VIU3->DMA_INC = 0; // 0 - noninterlaced


  VIU3->EXT_CONFIG =   VIU3_EXT_CONFIG_CS_EN_MASK * 0     // chroma swap enable=1
                 | VIU3_EXT_CONFIG_LENDIAN_MASK * 0   // little endian=1
                 | VIU3_EXT_CONFIG_RGB2YUV_EN_MASK * 0 // RGB->YUV conversion enable=1
                 | VIU3_EXT_CONFIG_DE_VALID_MASK * 0   //
                 | (4 << 5)                           // input format=4 - parallel RGB888, input format=5 - 8bit serial RGB888
                 | VIU3_EXT_CONFIG_PCLK_POL_MASK * 1  // pixel clock polarity
                 | VIU3_EXT_CONFIG_VSYNC_POL_MASK * 1 // VSYNC polarity
                 | VIU3_EXT_CONFIG_HSYNC_POL_MASK * 1 // HSYNC polarity
                 | VIU3_EXT_CONFIG_DE_POL_MASK * 0     // DE polarity
                 | VIU3_EXT_CONFIG_HMIRROR_EN_MASK * 0  // horizontal mirror enable
              ;

        // enable VSYNC interrupt      
        VIU3->SCR |= VIU3_SCR_VSYNC_EN_MASK | VIU3_SCR_VSYNC_IRQ_MASK ;

//VSYNC ISR
void vsyncISR(void)
{
    VIU3->SCR |= VIU3_SCR_DMA_ACT_MASK; // clear interrupt flags and start new DMA cycle
}

View solution in original post

0 Kudos
Reply
8 Replies
2,805 Views
kef2
Senior Contributor V

Weisong,

VIU3 supports two ITU input modes, four RGB input modes and one parallel YUV input mode, see 57.3 Video Input Signal Mapping.  ITU decoder block is used for ITU input mode. No quality is lost, unless you tell VIU3 to convert RGB888 to different formats.

2,805 Views
alfred_liu
NXP Employee
NXP Employee

Hi, Edward

could you tell how the VIU3 input RGB888 be sent out with RGB888 by VIU3?

VIU3.JPG

0 Kudos
Reply
2,805 Views
kef2
Senior Contributor V

Blocks 2,3,4 and 5 can be transparent and make no effect.

0 Kudos
Reply
2,805 Views
alfred_liu
NXP Employee
NXP Employee

Many thanks for your further information.

could you please guide us how we transparent Block 2,3,4 and 5?

any registers confiuration for it?

0 Kudos
Reply
2,806 Views
kef2
Senior Contributor V

Skiping IOMUXC configuration, you need to set up just few registers like below. I have no hardware to verify RGB888 settings, hope it works.

VIU3->SCR =   VIU3_SCR_MODE32BIT_MASK   * 1  // 32 bit mode
      | VIU3_SCR_ROUND_ON_MASK    * 0
      | VIU3_SCR_DITHER_ON_MASK   * 0
      | VIU3_SCR_DMA_ACT_MASK     * 0
      | VIU3_SCR_SCALER_EN_MASK   * 0
      | VIU3_SCR_YUV2RGB_EN_MASK  * 0
      | VIU3_SCR_BC_EN_MASK       * 0
      | VIU3_SCR_MODE444_MASK     * 0  // YUV444 vs YUV422
      | VIU3_SCR_ERROR_IRQ_MASK   * 0
      | VIU3_SCR_DMA_END_IRQ_MASK * 0
      | VIU3_SCR_VSTART_IRQ_MASK  * 0
      | VIU3_SCR_HSYNC_IRQ_MASK   * 0
      | VIU3_SCR_VSYNC_IRQ_MASK   * 0
      | VIU3_SCR_FIELD_IRQ_MASK   * 0
      | VIU3_SCR_ECC_EN_MASK      * 0
      | VIU3_SCR_ERROR_EN_MASK    * 0
      | VIU3_SCR_DMA_END_EN_MASK  * 0
      | VIU3_SCR_VSTART_EN_MASK   * 0
      | VIU3_SCR_HSYNC_EN_MASK    * 0
      | VIU3_SCR_VSYNC_EN_MASK    * 0
      | VIU3_SCR_FIELD_EN_MASK    * 0
      | VIU3_SCR_FORMAT_CTRL_MASK * 0 // replace 0 with required RGB888 byte order setting
      | VIU3_SCR_SOFT_RESET_MASK  * 0
                 ;

VIU3->DMA_ADDR = VIDEO_BASE; // address to store image data

VIU3->DMA_INC = 0; // 0 - noninterlaced


  VIU3->EXT_CONFIG =   VIU3_EXT_CONFIG_CS_EN_MASK * 0     // chroma swap enable=1
                 | VIU3_EXT_CONFIG_LENDIAN_MASK * 0   // little endian=1
                 | VIU3_EXT_CONFIG_RGB2YUV_EN_MASK * 0 // RGB->YUV conversion enable=1
                 | VIU3_EXT_CONFIG_DE_VALID_MASK * 0   //
                 | (4 << 5)                           // input format=4 - parallel RGB888, input format=5 - 8bit serial RGB888
                 | VIU3_EXT_CONFIG_PCLK_POL_MASK * 1  // pixel clock polarity
                 | VIU3_EXT_CONFIG_VSYNC_POL_MASK * 1 // VSYNC polarity
                 | VIU3_EXT_CONFIG_HSYNC_POL_MASK * 1 // HSYNC polarity
                 | VIU3_EXT_CONFIG_DE_POL_MASK * 0     // DE polarity
                 | VIU3_EXT_CONFIG_HMIRROR_EN_MASK * 0  // horizontal mirror enable
              ;

        // enable VSYNC interrupt      
        VIU3->SCR |= VIU3_SCR_VSYNC_EN_MASK | VIU3_SCR_VSYNC_IRQ_MASK ;

//VSYNC ISR
void vsyncISR(void)
{
    VIU3->SCR |= VIU3_SCR_DMA_ACT_MASK; // clear interrupt flags and start new DMA cycle
}

0 Kudos
Reply
2,805 Views
alfred_liu
NXP Employee
NXP Employee

Hi, Edward

Many thanks for your great support.

we also don't have hardware to varify it.

anyway the code will be very helpful for us.

I will colse the topic.

0 Kudos
Reply
2,805 Views
alfred_liu
NXP Employee
NXP Employee

many thanks Eward!

we will try your code.

0 Kudos
Reply
2,805 Views
alfred_liu
NXP Employee
NXP Employee

Hi, Edward

thanks for your information.

but how to explain the following information: ( I think the ITU decoder has limitation no matter the input are RGB888 or others.)

The format of active pixel data from the ITU stream is YUV 4:2:2. The decoder block can directly send

out this YUV 4:2:2 data, or interpolate it to YUV 4:4:4 format and send it out.


0 Kudos
Reply