Linux SDK for the i.Mx6 and I.mx5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Linux SDK for the i.Mx6 and I.mx5

4,951 Views
yudamr
Contributor II

I looking for Linux installation on Fedora machine , for I.Mx6 and I.Mx 5 .

can you provide me with Link for the SDK , and instruction for installation , and how to use the SDK environment.

thx

yuda

Labels (4)
5 Replies

2,499 Views
sanjayapalliker
Contributor I

Hi Yehuda Marko,

We suggest to use Ubuntu for iMX6 Linux development, and the documents are also based on Ubuntu.


You can use RidgeRun Linux SDK for FreeScale iMX6 Sabre SDP. Please follow the below link:

Getting Started Guide for iMX6 Sabre-SDP - RidgeRun Developer Connection

RidgeRun Linux SDK info for the Boundary devices SabreLite board is below :

Getting Started Guide for iMX6 SabreLite - RidgeRun Developer Connection

Please contact : sanjay@ridgerun.com For further support.

Thanks

Sanjay

RidgeRun Embedded Solutions

www.ridgerun.com

sanjay@ridgerun.com

0 Kudos
Reply

2,499 Views
LeonardoSandova
Specialist I

what do you mean by Linux SDK? Are you planing to develop apps for Android or LInux? i.Mx6 and I.mx6?

Leo

0 Kudos
Reply

2,499 Views
yudamr
Contributor II

I want to develop / bringup  Linux on custom board based on imx6.

so , I want to install the sdk or the relevant environment for build/compile etc .

my host machine is fedora.

thx

yuda

0 Kudos
Reply

2,499 Views
LeonardoSandova
Specialist I

As you may know, we are moving towards Yocto, so with it you can use most Linux distributions, including Fedora. With Yocto, you can install the toolchain and start generating binaries for your desired platform. For my point of point, it does not matter much the Linux Distribution, what it matters are the tools you are used to, so if those run fine in fedora, so you have the right setup.

Leo

2,499 Views
karina_valencia
NXP Apps Support
NXP Apps Support
Re: Linux SDK for the i.Mx6 and I.mx6

Qiang LiEmployee

We suggest to use Ubuntu for iMX Linux development, and the documents are also based on Ubuntu.

You can find all release software and document at "https://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6Q&webpageId=129226228141673454B...".