Memory controller setup for i.MX28 and i.MX50

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Memory controller setup for i.MX28 and i.MX50

18,125 Views
VladanJovanovic
NXP Employee
NXP Employee

Attached are files that will help with setting up i.MX28 and i.MX50 memory controller for different memory types.

 

Vladan

Original Attachment has been moved to: MX28_mDDR_register_programming_aid_v0.4.zip

Original Attachment has been moved to: MX50_DRAM_controller_register_programming_aid.zip

Labels (2)
9 Replies

14,593 Views
mliang
Contributor I

Hello,

 

I came across this discussion while searching for MX28 DDR2 register programming file.

We have 4 Micron MT47H256M8EB-25EIT on our board, total 1GByte, and running at about 130MHz. 

Currently we have some issues with our board.  We suspect it's the DDR2 memory issue and could be related to register setting.

I have setup the attached register programming file.  Can anyone please help and check to see if I have the registers setup correctly?

0 Kudos
Reply

14,593 Views
Yuri
NXP Employee
NXP Employee

Hello,

  I think, it makes sense to create separate request (to check memory configuration; also, please attach
(CPU <-> DRAM) schematic).

https://community.nxp.com/docs/DOC-329745  

Regards,

Yuri.

0 Kudos
Reply

14,593 Views
nobuyukitanaka
Contributor I

Is it correct in DQS_N_EN=1?

I think mDDR to be Single-ended DQS.

0 Kudos
Reply

14,593 Views
jschoen
Contributor III

Is there a similar ddr initialization aid for i.MX28 interfacing to DDR2?

I'm particularly interested in setting of HW_DRAM_CTL176 and how those should be set relative to Taond, Taofd, Taofpd, Taonpd, Tanpd, etc from the ddr2 datasheet.

0 Kudos
Reply

14,592 Views
Yuri
NXP Employee
NXP Employee

Please try the enclosed.

0 Kudos
Reply

14,592 Views
rohith1z
Contributor III

Is there a similar guide for imx25?

I'm working on supporting 256MB RAM (mddr) for this chipset and not sure if it's supports it.

section 24.1.9 of imx25 reference manual says Up to "128 Mbytes per chip select"

0 Kudos
Reply

14,592 Views
Yuri
NXP Employee
NXP Employee

SDRAM controller of the i.MX25 is relatively simple (when considering i.MX28 and i.MX50 ones),
nevertheless, the enclosed Excel example - hope - helps.

0 Kudos
Reply

14,592 Views
rohith1z
Contributor III

Thx for the quick response.

In particular I wanted to know if 256M of RAM is supported on a single chip select by mx25(I'm using a 4bank 16*16M ) H5MS1G62MFP-E3M

0 Kudos
Reply

14,592 Views
Yuri
NXP Employee
NXP Employee

I am afraid this is impossible to have 256 Mbytes with i.MX25, using single chip select.

There are the next restrictions of i.MX25 memory controller :

1) i.MX25 only can support 4-banks ;

2) i.MX25 has a 16-bit data bus ;

3) maximum Row address width is 14 bit ;

4) maximum Column address width is 10 bit.

This means maximum 128 Mbytes per CS.

0 Kudos
Reply