mpxy8300 basic code doesn't work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mpxy8300 basic code doesn't work

2,795 Views
configurehardwa
Contributor I

Hello,

i've got a problem with chip mpxy8300. I created blank project in codewarrior and try to set port:

 

#include <hidef.h> /* for EnableInterrupts macro */

#include "derivative.h" /* include peripheral declarations */

 

void main(void) {

 

 

PTADD=0x07;

PTAD=0x07;

 

 

 

  for(;;) {

   // __RESET_WATCHDOG(); /* feeds the dog */

  } /* loop forever */

  /* please make sure that you never leave main */

}

 


this code doesn't work. When i'm debugging it seems that uC don't go inside main function.


Does anybody know what i'm doing wrong.

Mirek

Labels (1)
0 Kudos
Reply
3 Replies

2,505 Views
configurehardwa
Contributor I

Thank's for your replies. Maybe it's a bug somewhere, i'm not so good programmer, can anybody try to find bug or help in other ways.

Regards

Mirek


/******************************************************************************

  FILE        : start08.c

  PURPOSE     : 68HC08 standard startup code

  LANGUAGE    : ANSI-C / INLINE ASSEMBLER

  ----------------------------------------------------------------------------

  HISTORY

    22 oct 93         Created.

    04/17/97          Also C++ constructors called in Init().

******************************************************************************/

/**********************************************************************/

/* NOTE:                                                              */

/* This version of the startup code assumes that main                 */

/* does never return (saving the 2 byte return address of _Startup on */

/* the stack).                                                        */

/**********************************************************************/

#define __NO_FLAGS_OFFSET   /* we do not need the flags field in the startup data descriptor */

#define __NO_MAIN_OFFSET    /* we do not need the main field in the startup data descriptor */

#include <start08.h>

#ifdef __cplusplus

#define __EXTERN_C  extern "C"

#else

#define __EXTERN_C

#endif

__EXTERN_C extern void main(void); /* prototype of main function */

#include "non_bank.sgm"

/***************************************************************************/

/* Macros to control how the startup code handles the COP:                 */

/* #define _DO_FEED_COP_   : do feed the COP                               */

/* Without defining any of these, the startup code does NOT handle the COP */

/***************************************************************************/

/* __ONLY_INIT_SP define:                                                  */

/* This define selects an shorter version of the startup code              */

/* which only loads the stack pointer and directly afterwards calls        */

/* main. This version does however NOT initialize global variables         */

/* (so this version is not ANSI compliant!).                               */

/***************************************************************************/

#if defined(_DO_FEED_COP_)

#define __FEED_COP_IN_HLI()  } _FEED_COP(); __asm {

#else

#define __FEED_COP_IN_HLI() /* do nothing */

#endif

#ifndef __ONLY_INIT_SP

#pragma DATA_SEG FAR _STARTUP

struct _tagStartup _startupData;    /* read-only:

                                     _startupData is allocated in ROM and

                                     initialized by the linker */

#pragma MESSAGE DISABLE C20001 /* Warning C20001: Different value of stack pointer depending on control-flow */

/* the function _COPY_L releases some bytes from the stack internally */

#if defined(__OPTIMIZE_FOR_SIZE__) || defined(_DO_FEED_COP_)

#pragma NO_ENTRY

#pragma NO_EXIT

#pragma NO_FRAME

/*lint -esym(528, loadByte) inhibit warning about unreferenced loadByte function */

static void near loadByte(void) {

  asm {

             PSHH

             PSHX

#ifdef __HCS08__

             LDHX    5,SP

             LDA     0,X

             AIX     #1

             STHX    5,SP

#else

             LDA     5,SP

             PSHA

             LDX     7,SP

             PULH

             LDA     0,X

             AIX     #1

             STX     6,SP

             PSHH

             PULX

             STX     5,SP

#endif

             PULX

             PULH

             RTS

  }

}

#endif /* defined(__OPTIMIZE_FOR_SIZE__) || defined(_DO_FEED_COP_) */

#ifdef __cplusplus

static void Call_Constructors(void) {

  int i;

#ifdef __ELF_OBJECT_FILE_FORMAT__

  i = (int)(_startupData.nofInitBodies - 1);

  while (i >= 0) {

    (&_startupData.initBodies->initFunc)[i]();  /* call C++ constructors */

    i--;

  }

#else /* __ELF_OBJECT_FILE_FORMAT__ */

  /* HIWARE object file format */

  if (_startupData.mInits != NULL) {

    _PFunc *fktPtr;

    fktPtr = _startupData.mInits;

    while(*fktPtr != NULL) {

      (**fktPtr)(); /* call constructor */

      fktPtr++;

    }

  }

#endif /* __ELF_OBJECT_FILE_FORMAT__ */

}

#endif

/*lint -esym(752,_COPY_L)  inhibit message on function declared, but not used (it is used in HLI) */

__EXTERN_C extern void _COPY_L(void);

/* DESC:    copy very large structures (>= 256 bytes) in 16-bit address space (stack incl.)

   IN:      TOS count, TOS(2) @dest, H:X @src

   OUT:

   WRITTEN: X,H */

#ifdef __ELF_OBJECT_FILE_FORMAT__

    #define toCopyDownBegOffs 0

#else

    #define toCopyDownBegOffs 2 /* for the hiware format, the toCopyDownBeg field is a long. Because the HC08 is big endian, we have to use an offset of 2 */

#endif

static void Init(void) {

/* purpose:     1) zero out RAM-areas where data is allocated

                2) init run-time data

                3) copy initialization data from ROM to RAM

*/

  /*lint -esym(529,p,i)  inhibit warning about symbols not used: it is used in HLI below */

  int i;

  int *far p;

  asm {

ZeroOut:

             LDA    _startupData.nofZeroOuts:1 ; // nofZeroOuts

             INCA

             STA    i:1                        ; // i is counter for number of zero outs

             LDA    _startupData.nofZeroOuts:0 ; // nofZeroOuts

             INCA

             STA    i:0

             LDHX   _startupData.pZeroOut      ; // *pZeroOut

             BRA    Zero_5

Zero_3:

             ; // CLR    i:1 is already 0

Zero_4:

             ; // { HX == _pZeroOut }

             PSHX

             PSHH

             ; // { nof bytes in (int)2,X }

             ; // { address in (int)0,X   }

             LDA    0,X

             PSHA

             LDA    2,X

             INCA

             STA    p                 ; // p:0 is used for high byte of byte counter

             LDA    3,X

             LDX    1,X

             PULH

             INCA

             BRA    Zero_0

Zero_1:

           ;  // CLRA   A is already 0, so we do not have to clear it

Zero_2:

             CLR    0,X

             AIX    #1

             __FEED_COP_IN_HLI()         ; // it's necessary to feed the COP in the inner loop for the fast COP timeout of some derivatives

Zero_0:

             DBNZA  Zero_2

Zero_6:

             DBNZ   p, Zero_1

             PULH

             PULX                     ; // restore *pZeroOut

             AIX    #4                ; // advance *pZeroOut

Zero_5:

             DBNZ   i:1, Zero_4

             DBNZ   i:0, Zero_3

CopyDown:

  }

  /* copy down */

  /* _startupData.toCopyDownBeg  --->  {nof(16) dstAddr(16) {bytes(8)}^nof} Zero(16) */

#if defined(__OPTIMIZE_FOR_SIZE__) || defined(_DO_FEED_COP_) /* for now: only -os version supports _DO_FEED_COP_ */

  asm {

#ifdef __HCS08__

             LDHX   _startupData.toCopyDownBeg:toCopyDownBegOffs

             PSHX

             PSHH

#else

             LDA    _startupData.toCopyDownBeg:(1+toCopyDownBegOffs)

             PSHA

             LDA    _startupData.toCopyDownBeg:(0+toCopyDownBegOffs)

             PSHA

#endif

Loop0:

             JSR    loadByte          ; // load high byte counter

             TAX                      ; // save for compare

             INCA

             STA    i

             JSR    loadByte          ; // load low byte counter

             INCA

             STA    i:1

             DECA

             BNE    notfinished

             CBEQX  #0, finished

notfinished:

             JSR    loadByte          ; // load high byte ptr

             PSHA

             PULH

             JSR    loadByte          ; // load low byte ptr

             TAX                      ; // HX is now destination pointer

             BRA    Loop1

Loop3:

Loop2:

             __FEED_COP_IN_HLI()

             JSR    loadByte          ; // load data byte

             STA    0,X

             AIX    #1

Loop1:

             DBNZ   i:1, Loop2

             DBNZ   i:0, Loop3

             BRA    Loop0

finished:

             AIS #2

    }

#else /*defined(__OPTIMIZE_FOR_SIZE__) || defined(_DO_FEED_COP_) */

  /* time optimized asm version. */

  asm {

#ifdef __HCS08__

             LDHX   _startupData.toCopyDownBeg:toCopyDownBegOffs

#else

             LDX    _startupData.toCopyDownBeg:(0+toCopyDownBegOffs)

             PSHX

             PULH

             LDX    _startupData.toCopyDownBeg:(1+toCopyDownBegOffs)

#endif

next:

             LDA   0,X                ; // list is terminated by 2 zero bytes

             ORA   1,X

             BEQ   copydone

             PSHX                     ; // store current position

             PSHH

             LDA   3,X                ; // psh dest low

             PSHA

             LDA   2,X                ; // psh dest high

             PSHA

             LDA   1,X                ; // psh cnt low

             PSHA

             LDA   0,X                ; // psh cnt high

             PSHA

             AIX   #4

             JSR   _COPY_L            ; // copy one block

             PULH

             PULX

             TXA

             ADD   1,X                ; // add low

             PSHA

             PSHH

             PULA

             ADC   0,X                ; // add high

             PSHA

             PULH

             PULX

             AIX   #4

             BRA next

copydone:

  }

#endif /* defined(__OPTIMIZE_FOR_SIZE__) || defined(_DO_FEED_COP_) */

  /* FuncInits: for C++, this are the global constructors */

#ifdef __cplusplus

  Call_Constructors();

#endif /* __cplusplus */

  /* implement ROM libraries initialization here (see startup.c) */

}

#endif /* __ONLY_INIT_SP */

#pragma NO_EXIT

__EXTERN_C void _Startup(void) {

/* set the reset vector to _Startup in the linker parameter file (*.prm):

    'VECTOR 0 _Startup'

    purpose:    1)  initialize the stack

                2)  initialize run-time, ...

                    initialize the RAM, copy down init data, etc (Init)

                3)  call main;

    called from: _PRESTART-code generated by the Linker

*/

  INIT_SP_FROM_STARTUP_DESC();

#ifndef  __ONLY_INIT_SP

  Init();

#endif

#ifndef __BANKED__

  __asm JMP main; /* with a C style main(); we would push the return address on the stack wasting 2 RAM bytes */

#else

  __asm CALL main;

#endif

}

0 Kudos
Reply

2,505 Views
mauriziostefane
Contributor II

Maybe there is a bug in basic project suggested by Freescale.

Try to stop the debugger at "Program Entry Point" instead of "User Specified: main" and go ahedd step by step to search for the problem.

I am using M5208EVB with Freescale demo example and It can't go to main because there is a bug in initialize_hardware() that jump at start again creating an infinite loop.

Regards

Maurizio

2,505 Views
BlackNight
NXP Employee
NXP Employee

Hello,

that sounds like indeed the controller has performed a reset.

Multiple possible reasons:

- watchdog: is the watchdog disabled?

- power supply: I have seen cases were an unstable power supply resets the chip.

- clock settings: if the problem happens during (wrong) clock initialization, the chip might get a wrong frequency and resets.

Hope this helps,

Erich