P&E USB BDM Rev.D problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

P&E USB BDM Rev.D problem

跳至解决方案
2,629 次查看
sebasira
Senior Contributor I

Hi all!

 

I've been working for years with several P&E BDM, and we have also break and repair some of them. But now, we receive 2 brand new BDM Rev.D and windows XP does not recognize any of them on 4 different computers, where all the other BDM we have work perfectly (BDM Rev.C)

 

We have USB 2.0 patch apply on the 4 PCs, and we use CW v3.1 and v4.6. When we connect the new BDM to the PC it doesn't appear under device manager. And the BDM LEDs remain off.

 

The strange thing is that accidentaly, we find out that if we connect the BDM to a USB hub, then the BDM works, That's strange, because the hub reduce USB speed. It's a chinesse hub with no external supply and it is USB 1.1.

 

We also try updating the BDM firmware. It said that it already has the latest, but we modify the firmware version number so we can force the change. We also load this firmware on the BDM revC and work without a problem.

 

One more thing, we ran the P&E Driver Test and all the files are detected

 

Can anybody help me here?

标签 (1)
标记 (5)
0 项奖励
回复
1 解答
2,389 次查看
sebasira
Senior Contributor I

Hi Tom!

Yes, it says "Enhanced Bus Controller".

For now, the only solution we found is to downgrade the BDM firmware from v5.84(latest) to v5.79

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,389 次查看
tom_thompson
Contributor III

Clearly there's some link with the USB version. Do your XP systems support USB 2.0?

To check, in the Device Manager, expand the USB Serial Bus Controller tree. For the Host Controller entries, if the word "enhanced" appears then it has USB 2.0. If not, it's USB 1.1.

---Tom

2,390 次查看
sebasira
Senior Contributor I

Hi Tom!

Yes, it says "Enhanced Bus Controller".

For now, the only solution we found is to downgrade the BDM firmware from v5.84(latest) to v5.79

0 项奖励
回复