K32W AN12798 bug2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

K32W AN12798 bug2

3,124 Views
danieltseng
Contributor V

< BLE test on ch2 >

二。Ch2.3.2.1 of AN12798, Frequency measurement also requires "continuous signal" ,

      As shown in the table, what kind of continuous signal can I choose?

pastedImage_2.png

pastedImage_1.png

Mentioned by Estephania as follows, using the following CW options, 

pastedImage_2.png

 

I feel very conflicted because ch2 is talking about "BLE Certi tool"

and ch3 is talking about "802.15.4 CMET".

In ch 2.3.2.1 BLE test, how could it be related to CMET(ch3) ?
How can BLE transmission be received by 802.15.4 CMET ?

Labels (1)
  • KW

0 Kudos
Reply
2 Replies

3,041 Views
Xiang_Li
NXP Employee
NXP Employee

>> Ch2.3.2.1 of AN12798, Frequency measurement also requires "continuous signal" ,

>> As shown in the table, what kind of continuous signal can I choose?

Test in AN12798, ch 2.3.2.1, is to test the accuracy of the frequency of the carrier wave.

In my opinion, the carrier wave can be either modulated or not modulated. But from the picture of the tool, it only shows modulated signals [2], [3], [4], [5], [6]. So you have to use a modulated signal for the test.

As for me I think any of the [2-6] is fine for the test. But if you look at AN12798 Annex C, it seems to suggest using [5] or [6] for test 2.3.2.1.

>> I feel very conflicted because ch2 is talking about "BLE Certi tool"

>> and ch3 is talking about "802.15.4 CMET".

It is not "BLE Certi tool", it is called "K32W Certi tool" in AN12798.

K32W is a product supporting 2 different RF technologies, BLE and 802.15.4. So there are 2 separate chapters explaining how to test BLE (ch2) and 802.15.4 (ch3) respectively.

>> In ch 2.3.2.1 BLE test, how could it be related to CMET(ch3) ?

No they are not related. How could ch2 related to ch3 if they are not even in the same chapter?

>> How can BLE transmission be received by 802.15.4 CMET ?

No BLE transmission cannot be received by 802.15.4 and vice versa, because they are different things.

3,041 Views
stephanie_m
NXP TechSupport
NXP TechSupport

Hello ,

I believe there is a confusion , could you please let me know what you are trying to do and why are you using this demo ? Are you performing some tests for the certification of the product? Are you trying to make a certification or radio tests for Bluetooth LE or 802.15.14?

Regards,

Estephania

0 Kudos
Reply