Config Microphone audio src by Dirana3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Config Microphone audio src by Dirana3

3,556 Views
yonghou
Contributor I

The microphone and dirana3 connection is like below:

Microphone             -->   Dirana3

-------------------------------------------------------

MICIN_D3_ADC2_P -> SAF775x: ADC2_IN  

MICIN_D3_ADC2_N-> SAF775x: ADC2_REF 

and Microphone audio will output from Dirana3: IIS_SD_OUT0  to SOC part.

my question is:

How to configure the dirana3 to make sure the microphone source can route from ADC2_IN/REF to IIS_SD_OUT0 ?

in another words: How to  do configuration of the dirana#3 to support MIC -> dirana -> SOC ?

Labels (1)
Tags (1)
0 Kudos
Reply
3 Replies

3,275 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, YongHou,

Regarding your question, I suppose that you use SAF or TDF radio families, unfortunately, this is DSC formula, we do not support the radio family, I am sorry.

BR

Xiangjun Rong

0 Kudos
Reply

3,275 Views
tobin_tomy
Fresh Out Contributor

@ xiangjun.rong Can you Suggest, which group is supporting for SAF Families? Even I am also looking into the same ?

0 Kudos
Reply

3,275 Views
tobin_tomy
Fresh Out Contributor

Hi Xiangjun,

In Dirana 3, we have 2 EPIC cores and 1 Hifi core is there for Audio Processing. As per my initial level of understanding, EPIC cores will take care about the audio routing by some framework API's. I would like to know how the Audio Samples will be processed from Mic---ADC--Receiver--DSP---Transmitter--DAC---Speakers? Is there any Interrupt based DMA/EMDMA in between that? Since I am new to Dirana 3, It would be helpful if you are able to suggest some supportive document for the same. Thanks in Advance.

0 Kudos
Reply