This is the procedure and patch to set up Ubuntu 13.10 64bit Linux Host PC and building i.MX6x L3.0.35_4.1.0. It has been tested to build GNOME profile and with FSL Standard MM Codec for i.MX6Q SDB board.
A) Basic Requirement:
B) Installed the needed packages to the Linux Host PC
$ sudo apt-get update
$ sudo apt-get install gettext libgtk2.0-dev rpm bison m4 libfreetype6-dev
$ sudo apt-get install libdbus-glib-1-dev liborbit2-dev intltool
$ sudo apt-get install ccache ncurses-dev zlib1g zlib1g-dev gcc g++ libtool
$ sudo apt-get install uuid-dev liblzo2-dev
$ sudo apt-get install tcl dpkg
$ sudo apt-get install asciidoc texlive-latex-base dblatex xutils-dev
$ sudo apt-get install texlive texinfo
$ sudo apt-get install lib32z1 lib32ncurses5 lib32bz2-1.0
$ sudo apt-get install libc6-dev-i386
$ sudo apt-get install u-boot-tools
$ sudo apt-get install scrollkeeper
$ sudo apt-get install gparted
$ sudo apt-get install nfs-common nfs-kernel-server
$ sudo apt-get install git-core git-doc git-email git-gui gitk
$ sudo apt-get install meld atftpd
$ sudo ln -s /usr/lib/x86_64-linux-gnu/librt.so /usr/lib/librt.so
C) Unpack and install the LTIB source package and assume done on the home directory:
$ cd ~
$ tar -zxvf L3.0.35_4.1.0_130816_source. tar.gz
$ ./L3.0.35_4.1.0_130816_source/install
After that, you will find ~/ltib directory created
D) Apply the patch to make L3.0.35_4.1.0 could be installed and compiled on Ubuntu 13.10 64bit OS
$ cd ~/ltib
$ git apply 0001_make_L3.0.35_4.1.0_compile_on_Ubuntu_13.10_64bit_OS.patch
What the patch is doing:
a) The patch modifies the following files:
b) Add the following files to the pkgs directory:
E) Then, it is ready to proceed the rest of the LTIB env setup process:
$ cd ~/ltib
$ ./ltib -m config
$ ./ltib
Reference:
1. https://github.com/hashdist/hashstack/commit/f6be2a58de62327d05e052d89c9aa931d4c926b3
2. https://github.com/hashdist/hashstack/issues/81
NOTE:
When compiling gstreamer, this warning was pop up. Just ignore it seems okay.