LPC804: PLU Hands-on Lab Guide

Document created by Carlos_Mendoza Employee on Nov 15, 2018Last modified by Carlos_Mendoza Employee on Nov 15, 2018
Version 2Show Document
  • View in full screen mode

 

Hello Community!


This document is provided as a hands-on lab guide.  The intent of the lab is to demonstrate how to program the LPCXpresso804 board with the MCUXpresso IDE making use of the SDK examples and the PLU module drivers.

 

The PLU configuration tool will be used to create a new schematic design that will be programmed to the PLU.

 

Setup
The following items need to be installed on your computer to complete the lab:

 

Software:

 

•    SDK_2.4.1_LPCXpresso804:

-    Copy link into browser: https://mcuxpresso.nxp.com/en/select?device=LPCXpresso804

-    Select ‘MCUXpresso IDE’ or ‘All Toolchains’ in the Toolchain IDE drop-down
-    Select ‘Download SDK’

 

•    MCUXpresso IDE version 10.2.1:

-    Can be installed at following link: https://www.nxp.com/mcuxpresso/ide

 

•    PLU configuration tool

-    Can be installed at this link: https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/i.mx-applications-processors/i.mx-rt-series/i.mx-rt1060-crossover-processor-with-arm-cortex-m7-core:i.MX-RT1060?tab=Design_Tools_Tab


 
Hardware:


•    LPCXpresso804 Development Board (OM40001): https://www.nxp.com/support/developer-resources/evaluation-and-development-boards/lpcxpresso-boards/lpcxpresso804-for-the-lpc804-family-of-mcus:OM40001?tab=Design_Tools_Tab

 

•    PLU Shield Board


•    1 Micro USB cable

 

Hope this guide is helpful! Any comments are welcome.

 

Best Regards,
Carlos Mendoza
Technical Support Engineer

Attachments

Outcomes