Example MPC5644A BookE PinToggle - S32DS Power 2017.R1

File uploaded by stanish Employee on May 9, 2018Last modified by stanish Employee on May 9, 2018
Version 4Show Document
  • View in full screen mode

This application shows how to  build and debug BOOKE based project.

It contains BOOKE startup/ISR code and it is compiled to generate non-VLE BOOKE code.

 

Note:

Before running this project please make sure your startup script is configuring MMU to use BOOKE instructions.

The script is typically located here: "c:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.7.3.201803261737\win32\gdi\P&E\s32e200_mpc564xa.mac"

The plugin version folder may differ.

The updated script is part of attached ZIP archive.

Outcomes