Example MPC5602D FMPLL GHS614

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example MPC5602D FMPLL GHS614

Example MPC5602D FMPLL GHS614

********************************************************************************

* Detailed Description:

* Application performs basic initialization, setup PLL to maximum allowed frequency (48MHz)

* Setup SIU, and demonstrate frequency modulation.

* ------------------------------------------------------------------------------

* Test HW:        XPC560B 64LQFP, XPC56XX EVB MOTHEBOARD Rev.C

* MCU:             SPC5602D

* Cut:               1M18Y

* Fsys:             48 MHz

* Debugger:     Lauterbach Trace32

* Target:           internal_FLASH

* EVB clkout pin : Port J7 - pin 0

*

********************************************************************************

157764_157764.png

Labels (1)
Attachments
No ratings
Version history
Last update:
‎08-02-2016 12:17 AM
Updated by: