All Boards Serial Console

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

All Boards Serial Console

All Boards Serial Console

Minicom

     

It's a simple terminal program, easy to configure and use. Can be downloaded and installed from your Linux package distribution (Synaptic, apt-get, yum) or through this link.

     

Minicom is a terminal emulation that can access a remote serial console enabling the configuration of Bootloader or the flash file system of the board.

 

Configuring

     

Run Minicom calling it from Terminal:

   

$ minicom 

     

Reach the cofiguration by typing CTRL-A Z

Press key Z after releasing CTRL and A.

Configure Minicom to work with i.MX, follow the procedure below.

 

Set the Serial Port

     

At the screen configuration, type O, choosing Configure Minicom

In menu, choose Serial Port Setup

Below, the configuration option:

     

+-----------------------------------------------------------------------+

| A - Serial Device  : /dev/ttyS0                            |

| B - Lockfile Location  : /var/lock                          |

| C - Callin Program  :                                          |

| D - Callout Program  :                                        |

| E - Bps/Par/Bits  : 115200 8N1                          |

| F - Hardware Flow Control : No                          |

| G - Software Flow Control : No                            |

|                                                                        |

| Change which setting?                                      |

+-----------------------------------------------------------------------+

     

Type the letter of option to enable the modification.

Remember to choose the right Serial Device.


Screen

     

Another useful program to use with serial ports is screen.

It is a screen manager with VT100/ANSI terminal emulation usually available in Linux distributions.

To open serial device /dev/ttyS0, for example, using 115200 baudrate, simply use:

   

$ screen /dev/ttyS0 115200 

     

To kill the screen manager, use Ctrl + a, k.

For a list of useful parameters and commands, try:

   

$ man screen 
标签 (1)
无评分
版本历史
最后更新:
‎09-10-2020 02:44 AM
更新人: